Write/Read |
About Pulse Measurements |
Description |
When set to OFF, the improved software gating sensitivity is turned OFF and all data outside the measurement band is zeroed. This setting is used for troubleshooting purposes. There is NO user-interface control for this setting. |
VB Syntax |
pulseMeas.SoftwareGateState = bool |
Variable |
(Type) - Description |
|
pulseMeas |
A PulseMeasurementControl (object) |
|
bool |
True - Turn ON software gating. False - Turn OFF software gating. |
Return Type |
Boolean |
Default |
True |
Examples |
pulse.SoftwareGateState = True 'Write |
|
value = pulse.SoftwareGateState 'Read |
|
C++ Syntax |
HRESULT get_SoftwareGateState(VARIANT_BOOL *pVal); HRESULT put_SoftwareGateState(VARIANT_BOOL newVal); |
Interface |
IPulseMeasurementControl2 |