Read only |
About VNA Options |
Description |
Returns the number of ports that can output a signal. To learn more, see Remotely Specifying a Source Port. |
VB Syntax |
value = object.SourcePortCount |
Variable |
(Type) - Description |
|
value |
(Long) - Variable to store the returned integer value of the number of source ports. |
|
object |
A Channel (object)- always more complete than capabilities object. A Capabilities (object) - use when a channel is not available, or to find the common ports across all channels. |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = chan.SourcePortCount 'Read |
C++ Syntax |
HRESULT get_SourcePortCount(long * count ); |
Interface |
IChannel13 ICapabilities4 |