Write/Read |
About NFX |
Description |
Enables and disables the use of source pull technique to compute S22 on Noise Figure on Converters. Learn more. |
VB Syntax |
nfx.SourcePullForSParameters = value |
Variable |
(Type) - Description |
|
nfx |
A NoiseFigure (object) |
|
value |
(Boolean) Source pull technique state. Choose from: False - Disable use of source pull technique. True - Enable use of source pull technique. |
Return Type |
Boolean |
Default |
False |
Examples |
nfx.SourcePullForSParameters = true 'Write |
|
sourcePull = nfx.SourcePullForSParameters 'Read |
|
C++ Syntax |
HRESULT get_SourcePullForSParameters (VARIANT_BOOL * Val) HRESULT put_SourcePullForSParameters (VARIANT_BOOL newVal) |
Interface |
INoiseFigure4 |