Write/Read |
About Power Limit |
Description |
Enables and disables Global Power Limiting for the specified port. |
VB Syntax |
gpl.State(port) = bool |
Variable |
(Type) - Description |
|
gpl |
A GlobalPowerLimit (object) |
|
port |
(Long) Port number for which power limit state is to be set. |
|
bool |
(Boolean) Choose from: True - Power Limiting is enabled. False - Power Limiting is disabled. |
Return Type |
Boolean |
Default |
False |
Examples |
gpl.State(1) = True 'Write |
|
Limit = gpl.State(2) 'Read |
|
C++ Syntax |
HRESULT get_State(long port, VARIANT_BOOL *pVal) |
Interface |
IGlobalPowerLimit |