Read/Write |
Learn about Calibration Thru Methods |
Description |
This command is replaced by PathThruMethod Property. Sets and returns the method for performing the Cal Method and the THRU portion of the calibration. |
VB Syntax |
guidedCal.ThruCalMethod = value |
Variable |
(Type) - Description |
|
guidedCal |
GuidedCalibration (object) |
|
value |
(Enum as NAThruCalMethod) Choose from: 0 - naDefaultCalMethod - allow the VNA to choose the best possible method (from the following) depending on whether the device or ECal module is insertable or non-insertable and given the model number of the VNA. (default selection if omitted.) 1 - naAdapterRemoval - Perform Adapter removal calibration. 2 - naFlushThru - Perform Flush Thru calibration. 3 - naDefinedThru - Perform Defined Thru calibration. If performing an ECal, this is the Thru standard in the ECal module. 4 - naUnknownThru - Perform Unknown Thru calibration. 5 - naSOLT - Perform SOLT calibration 6 - naTRL - Perform TRL calibration 7 - naQSOLT - Perform QSOLT calibration. |
Return Type |
Enum |
Default |
0 - naDefaultCalMethod |
Examples |
guided.ThruCalMethod = naDefinedThru |
C++ Syntax |
HRESULT get_ThruCalMethod(enum NAThruCalMethod *thruMethod); HRESULT put_ThruCalMethod(enum NAThruCalMethod thruMethod); |
Interface |
IGuidedCalibration |