Write/Read |
About PNA-X Touchscreen |
Description |
Sets and reads the state of the PNA-X Touchscreen (ON and OFF). This setting remains until changed again from the front-panel or remote command. |
VB Syntax |
app.Touchscreen = state |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
state |
(boolean) False (0) - Disables use of Touchscreen True (1) - Enables use of Touchscreen |
Return Type |
Boolean False - OFF True - ON |
Default |
TRUE when shipped from factory. |
Examples |
app.Touchscreen = True 'Write |
|
coupl = app.Touchscreen 'Read |
|
C++ Syntax |
HRESULT put_Touchscreen(VARIANT_BOOL bState) HRESULT get_Touchscreen(VARIANT_BOOL *bState) |
Interface |
IApplication12 |