Screen Tour


Click on image areas to learn more.

Change VNA Display Settings

The VNA display is controlled by a third-party display driver. This driver is capable of producing many display effects which are beyond the basic needs of the VNA measurement environment. Keysight does not specify or warrant these display settings.

WARNING: The VNA display must remain in the 16 bit color setting in order to comply with international emissions regulations.

Restore VNA Display Settings

When using external programs to control the VNA, it is possible that the display settings may become corrupt. When this occurs, the following will restore the VNA display settings:

See Also


About the Touchscreen

The VNA is equipped with a 12.1-inch Hi resolution, color, touch-sensitive LCD screen for displaying traces, softkeys, and other measurement related information. The touch screen LCD allows you to make measurement settings by touching the LCD screen directly with a finger.

Important

  • Do not press the surface of the LCD screen with a sharp object such as a pen. This will damage the LCD screen surface or cause the screen to fail.

  • Occasionally, a few pixels may appear on the screen as a fixed point of blue, green or red. This is not a failure of the LCD screen and does not affect the performance of your product.

  • Because of the LCD screen, burn-in is not likely. In addition, we do not recommend using a screen-saver on the VNA.

 

How to Calibrate or turn ON | OFF the Touchscreen

Programming Commands

Using Hardkey/SoftTab/Softkey

To turn Touchscreen ON or OFF:

  1. Press Display > Display Setup.

  2. Click Touchscreen to turn ON/OFF.

To calibrate Touchscreen:

Note: The Touchscreen is self calibrating and should not require calibration. However, if the touch locations are not accurate, perform the following procedure to calibrate the Touchscreen.

  1. For Windows 7, perform the following procedure.

    1. In the PNA application, press System > Main > Control Panel.

    2. In the Control Panel, select Hardware and Sound > Tablet PC Settings > Calibrate the screen for pen or touch input.

  2. For Windows 10, perform the following procedure.

    1. Close the PNA application.

    2. Press or select the Windows key on an external keyboard, or click on the Windows Start icon in the lower-left corner.

    3. Select Settings to access the Settings dialog.

    4. In the search field of the Settings dialog, type calibrate then select Calibrate the screen for pen or touch input.

    5. The Tablet PC Settings dialog is displayed:

    6. Select the Display tab.

    7. Click on the Calibrate... button.

    8. In the User Account Control dialog, click Yes.

    9. Follow the instructions displayed on the screen.

To calibrate Touchscreen when external monitor is connected to PNA:

When a second monitor is added to a Windows PC where the primary monitor has a touchscreen, Windows may associate touch inputs with the window shown on the extended monitor rather than on the monitor that has the touchscreen. Since the computer in a PNA runs on the Windows operating system, the PNA can exhibit this condition.

Note: The Touchscreen is self calibrating and should not require calibration. However, if the touch locations are not accurate, perform the following procedure to calibrate the Touchscreen.

  1. Minimize the PNA application window by selecting File then Minimize Application.

  2. Press or select the Windows key on an external keyboard, or click on the Windows Start icon in the lower-left corner.

  3. Select Settings to access the Settings dialog.

  4. In the search field of the Settings dialog, type calibrate then select Calibrate the screen for pen or touch input.

  5. The Tablet PC Settings dialog is displayed:

  6. Select the Display tab.

  7. Click on the Setup... button. At this point, both the PNA screen and the external monitor will display a white background. Only one screen will also display the following message
    :
    Touch the screen to identify it as the touchscreen.
    If this is not the Tablet PC Screen, press Enter to move to the next screen. To close tool, press Esc.

  8. If the message is on the PNA screen, touch the screen. The calibration is now finished and the Calibrate touch dialog will reappear. Press OK.

  9. If the message is not on the PNA screen, press Enter on the external keyboard until the message is displayed on the PNA screen. Touch the PNA screen, then press OK on the Calibrate touch dialog.

Note: If the calibration makes the touch operation worse, click on the Reset button in the Tablet PC Settings dialog to reset the calibration data.

The touchscreen ON |OFF setting remains until changed again from this menu, the Preferences dialog, or remotely.

Active Entry

Allows you easily select the tools. Learn more.

Trace Status

Provides details of each trace in the window. Highlighted trace indicates the active trace. Learn more.

Entry Toolbar

Along with the softkeys, allows numeric values to be entered for settings. Learn about all toolbars.

Marker Readout

Provides stimulus and response information for markers. Learn about customizing the marker readout area. See also Marker Drag.

Softkeys

The combination of hardkeys and softkeys allows easy access to all VNA features without a mouse.

SoftTabs

Pressing these tabs will display corresponding softkeys.

Hardkeys

Performs interface operations that are equivalent to those of keys in the INSTRUMENT keys, RESPONSE keys, STIMULUS keys and UTILITY keys on the front panel of VNA. Learn more.

Window Number

Provides window identification which is useful for remote programmers.

Status Bar

Provides detail about all aspects of the status of the analyzer. Learn more.

Stimulus Range

Displays the start and stop values of the sweep range.

Softkey Toolbar

These icons provide shortcuts to quickly select the softkey tools. Learn more.

Marker Drag

Drag a displayed marker across the trace using a finger (with touchscreen ON) or a mouse. Learn more.

Expanded Mouse Capabilities

Windows

Traces

Markers

Softkeys

Softkey Annotations

Item

Description

Menu...

Selection launches a dialog box.

Menu

Selection launches another level of softkeys.

Item

Indicates the item (marker, trace, window) is ON. Any number of objects can be ON.

Item

Indicates the item (marker, trace, window) is OFF. Click to turn item ON.

Item

Indicates the item IS selected.

Item

Indicates the item is NOT selected. Click to select. Only one item in the collection can be ON.

* Item

Enter value in Entry toolbar.

Item
on |OFF

Capitalization indicates the current setting.