Reads Gain Compression data from the current Gain Compression acquisition.
These commands are Superseded by the CALCulate:MEASure:GCData commands.
|
CALCulate:GCData: |
Click on a keyword to view the command details.
The calibration commands listed in this topic are supplemental to the Guided Cal commands.
CALC:CUSTom:DEFine - creates a gain compression measurement.
SENS:GCSetup - Most Gain Compression settings.
CALC:GCMeas:ANAL - Gain Compression Analysis settings
Gain compression data can also be saved to a *.csv file. Learn how.
See Also
|
Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Only) Returns measurement data at all frequency and power data points for GCA SMART sweeps and 2D sweeps.
Use Calc:Data? to return just the displayed data results (not the background sweeps). A compression parameter must be present. Learn more. The format of the data is the same as the format of the measurement that you select using Calc:Par:Select. If the measurement is scalar, than one number is returned per sweep per data point. If complex (such as Smith Chart format) than both real and imaginary numbers are returned. If correction is on, corrected data are returned. Otherwise, raw data are returned. |
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<param> |
(String) Parameter to read. NOT Case-sensitive. The specified parameter need NOT be displayed or selected. However, a compression parameter must be present. Learn more. Choose from:
|
|
Examples |
data = CALC:GCD:DATA? "pin" data = calculate:gcdata:data? "pout" |
|
Return Type |
Array of data |
|
Not Applicable |
|
|
Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Only) For a specified data point, returns the imaginary part of the specified Gain Compression data. If correction is on, corrected data are returned. Otherwise, raw data are returned. Can be used with Smart and 2D sweeps.
|
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from:
|
|
<dPoint> |
Data point (FREQ or POWer) for which data is returned. |
|
<param> |
(String) Parameter to read. NOT Case-sensitive. The specified parameter need NOT be displayed. However, a compression parameter must be present. Learn more.
|
|
Examples |
For the fifth frequency data point, returns 'Power Output' imaginary (phase) data from all power stimulus values. For SmartSweep, if there are 30 power sweep points, 30 values are returned. For 2D sweeps, 30 or 31 power sweep points may be returned. Learn more. data = CALC:GCD:IMAG? FREQ,5,"pout" |
|
Return Type |
Array of data |
|
Not Applicable |
|
|
Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-only) In a SMART sweep, returns the max number of iterations that it took for ALL frequencies to converge. Use this number to determine the size of the block data that is returned from Gain Compression SMART sweep data queries. For a 2D sweep, returns the number of power points. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
data = CALC:GCD:ITER? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Only) For a specified data point, returns the real part of the Gain Compression data. If correction is on, corrected data are returned. Otherwise, raw data are returned. Can be used with Smart and 2D sweeps.
|
|
|
Parameters |
|
|
<ch> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Choose from:
|
|
<dPoint> |
Data point (FREQ or POWer) for which data is returned. |
|
<param> |
(String) Parameter to read. NOT Case-sensitive. The specified parameter need NOT be displayed. However, a compression parameter must be present. Learn more.
|
|
Examples |
For the fifth frequency data point, returns 'Power Output' real data from all power stimulus values. For SmartSweep, if there are 30 power sweep points, 30 values are returned. For 2D sweeps, 30 or 31 power sweep points may be returned. Learn more. data = CALC:GCD:REAL? FREQ,5,"pout" |
|
Return Type |
Array of data |
|
Not Applicable |
|