CALCulate:MEASure:FUNCtion DOMain | USER | [:RANGe] | STARt | STOP STATistics | [:STATe] |
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-only) Returns the trace statistic data for the selected statistic type for the specified channel. Select the type of statistic with CALC:MEAS:FUNC:TYPE. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Return Type |
Depends on FORM:DATA |
Example |
|
Not applicable |
|
Applicable Models: All (Read-Write) Sets the range used to calculate trace statistics. Each channel has 16 user ranges. The x-axis range is specified with the CALC:MEAS:FUNC:DOM:USER:START and STOP commands. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<range> |
Range number. Choose from: 0 to 16 0 is Full Span of the current x-axis range 1 to 16 are user-specified ranges |
Examples |
CALC:MEAS2:FUNC:DOM:USER
4 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER[:RANGe]? |
Return Type |
Numeric |
0 - Full Span |
|
Applicable Models: All (Read-Write) Sets the start of the specified user-domain range. To apply this range, use CALC:MEAS:FUNC:DOM:USER To set the stop of the range, use CALC:MEAS:FUNC:DOM:USER:STOP. Note: This command does the same as CALC:MEAS:MARK:FUNC:DOM:USER:STAR |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<range> |
Range number that will receive the start value. Choose an integer between 1 and 16 |
<start> |
Start value of the specified range.
Choose a real number between: |
Examples |
CALC:MEAS2:FUNC:DOM:USER:STAR
1,1e9 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER:STARt? <range> |
Return Type |
Numeric |
The analyzer's Minimum x-axis value |
|
Applicable Models: All (Read-Write) Sets the stop value of the specified user-domain range. To apply this range, use CALC:MEAS:FUNC:DOM:USER. To set the start of the range, use CALC:MEAS:MARK:FUNC:DOM:USER:STAR Note: This command does the same as CALC:MEAS:MARK:FUNC:DOM:USER:STOP |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<range> |
Range number that will receive the stop value. Choose an integer between 1 and 16 |
<stop> |
Stop value of the specified range.
Choose a real number between: |
Examples |
CALC:MEAS2:FUNC:DOM:USER:STOP
4,5e9 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER:STOP? <range> |
Return Type |
Numeric |
The analyzer's Maximum x-axis value |
|
Applicable Models: All (Write-only) For the active trace of specified channel, executes the statistical analysis specified by the CALC:MEAS:FUNC:TYPE command. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:FUNC:EXEC |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Displays and hides the trace statistics (peak-to-peak, mean, standard deviation) on the screen. The analyzer will display either measurement statistics or Filter Bandwidth statistics; not both. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<ON|OFF> |
ON - Displays trace statistics OFF - Hides trace statistics |
Examples |
CALC:MEAS2:FUNC:STAT
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:STATistics[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF (0) |
|
Applicable Models: All (Read-Write) For Smith Chart format, changes trace statistics (peak-to-peak, mean, standard deviation) units from Log Mag (dB) to impedance (ohms) on the screen. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<ON|OFF> |
ON - Units displayed in ohms OFF - Units displayed in dB |
Examples |
CALC:MEAS2:FUNC:STAT:RES ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:STATistics:RESistance[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF (0) |
|
Applicable Models: All (Read-Write) Sets statistic TYPE that you can then query using CALC:MEAS:FUNCtion:DATA?. Note: This command affects only the selected measurement on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<char> |
Choose from: PTPeak - the difference between the max and min data points on the trace. STDEV - standard deviation of all data points on the trace MEAN - mean (average) of all data points on the trace MIN - lowest data point on the trace MAX - highest data point on the trace |
Examples |
CALC:MEAS2:FUNC:TYPE
PTP |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FUNCtion:TYPE? |
Return Type |
Character |
PTPeak |
|