These commands are Superseded by the CALCulate:MEASure:FUNCtion commands.
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Returns the trace statistic data for the selected statistic type for the specified channel. Select the type of statistic with CALC:FUNC:TYPE. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Return Type |
Depends on FORM:DATA |
Example |
|
Not applicable |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the range used to calculate trace statistics. Each channel has 16 user ranges. The x-axis range is specified with the CALC:FUNC:DOM:USER:START and STOP commands. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<range> |
Range number. Choose from: 0 to 16 0 is Full Span of the current x-axis range 1 to 16 are user-specified ranges |
Examples |
CALC:FUNC:DOM:USER
4 |
Query Syntax |
CALCulate<cnum>:FUNCtion:DOMain:USER[:RANGe]? |
Return Type |
Numeric |
0 - Full Span |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the start of the specified user-domain range. To apply this range, use CALC:FUNC:DOM:USER To set the stop of the range, use CALC:FUNC:DOM:USER:STOP. Note: This command does the same as CALC:MARK:FUNC:DOM:USER:STAR |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<range> |
Range number that will receive the start value. Choose an integer between 1 and 16 |
<start> |
Start value of the specified range.
Choose a real number between: |
Examples |
CALC:FUNC:DOM:USER:STAR
1,1e9 |
Query Syntax |
CALCulate<cnum>:FUNCtion:DOMain:USER:STARt? <range> |
Return Type |
Numeric |
The analyzer's Minimum x-axis value |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the stop value of the specified user-domain range. To apply this range, use CALC:FUNC:DOM:USER. To set the start of the range, use CALC:FUNC:DOM:USER:START Note: This command does the same as CALC:MARK:FUNC:DOM:USER:STOP |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<range> |
Range number that will receive the stop value. Choose an integer between 1 and 16 |
<stop> |
Stop value of the specified range.
Choose a real number between: |
Examples |
CALC:FUNC:DOM:USER:STOP
4,5e9 |
Query Syntax |
CALCulate<cnum>:FUNCtion:DOMain:USER:STOP? <range> |
Return Type |
Numeric |
The analyzer's Maximum x-axis value |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Write-only) For the active trace of specified channel, executes the statistical analysis specified by the CALC:FUNC:TYPE command. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:FUNC:EXEC |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Displays and hides the trace statistics (peak-to-peak, mean, standard deviation) on the screen. The analyzer will display either measurement statistics or Filter Bandwidth statistics; not both. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<ON|OFF> |
ON - Displays trace statistics OFF - Hides trace statistics |
Examples |
CALC:FUNC:STAT
ON |
Query Syntax |
CALCulate<cnum>:FUNCtion:STATistics[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF (0) |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets statistic TYPE that you can then query using CALC:FUNCtion:DATA?. Note: This command affects only the selected measurement on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<char> |
Choose from: PTPeak - the difference between the max and min data points on the trace. STDEV - standard deviation of all data points on the trace MEAN - mean (average) of all data points on the trace MIN - lowest data point on the trace MAX - highest data point on the trace |
Examples |
CALC:FUNC:TYPE
PTP |
Query Syntax |
CALCulate<cnum>:FUNCtion:TYPE? |
Return Type |
Character |
PTPeak |
|