Controls the color settings of the VNA display.
DISPlay:COLor TRACe | DATA | MARKer | MEMory | MMARker
|
Click on a keyword to view the command details.
See Also
Applicable Models: All (Read-Write) Set and return the background color for the active window on the VNA display or hardcopy print. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:ABAC 10,10,10 display:color1:abackground 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:ABACkground? |
Return Type |
Numeric (n,n,n) |
Display = 0,0,24 (Black) Print = 255,255,255 (White) |
|
Applicable Models: All (Read-Write) Set and return the background color for the inactive windows on the VNA display or hardcopy print. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:BACK 10,10,10 display:color1:background 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:BACKground? |
Return Type |
Numeric (n,n,n) |
Display = 0,0,0 (Black) Print = 255,255,255 (White) |
|
Applicable Models: All (Read-Write) Set and return the labels and grid frame colors in the active window for the VNA display or hardcopy print. (Active labels, Grid frame) |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:GRAT1 10,10,10 display:color1:grat1 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:GRAT1? |
Return Type |
Numeric (n,n,n) |
Display = 175,175,175 Print = 0,0,0 (Black) |
|
Applicable Models: All (Read-Write) Set and return the inner lines of all grid in all windows, and the grid frame in inactive windows for the VNA display or hardcopy print. (GRID) |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:GRAT2 10,10,10 display:color1:grat2 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:GRAT2? |
Return Type |
Numeric (n,n,n) |
Display = 100,100,100 Print = 50,50,50 |
|
Applicable Models: All (Read-Write) Set and return the Inactive (not selected) Window Labels for the VNA display or hardcopy print. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:ILAB 10,10,10 display:color1:ilabel 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:ILABel? |
Return Type |
Numeric (n,n,n) |
Display = 160,160,160 Print = 0,0,0 (Black) |
|
Applicable Models: All (Read-Write) Set and return the limit line color of failed traces or failure indicators (dots) and the word Fail. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:LIM1 10,10,10 display:color1:lim1 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:LIM1? |
Return Type |
Numeric (n,n,n) |
Display = 255,20,20 Print = 255,20,20 |
|
Applicable Models: All (Write-only) Load a color theme from a disc file. |
|
Parameters |
|
<n> |
Colors to load. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<value> |
String. Filename of the stored theme. The .colors suffix is automatically appended. By default, files are stored in C:\Program Files(x86)\Keysight\Network Analyzer\Colors\. To store and load files from a different folder, specify the full path and filename. |
Examples |
DISP:COL:LOAD "myDisplayTheme" display:color2:load "myPrintTheme" |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Write-only) Resets the current theme to the default VNA colors. |
|
Parameters |
|
<n> |
Colors to reset. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
Examples |
DISP:COL:RES display:color2:reset |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Write-only) Saves the current color theme to a disc file. |
|
Parameters |
|
<n> |
Colors to store. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<value> |
String. Filename. The .colors suffix is automatically appended. By default, files are stored in C:\Program Files(x86)\Keysight\Network Analyzer\Colors\. To store and load files from a different folder, specify the full path and filename. |
Examples |
DISP:COL:STOR "myDisplayTheme" display:color2:store "myPrintTheme" |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Set and return the color of Data and Limit Lines for nth trace in a window. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<nth> |
Numeric. Relative trace number in the window for which colors are set. This is not necessarily the trace number. Learn more. Choose from 1 to 8. If unspecified, <nth> is set to 1 (first trace). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:TRAC2:DATA 10,10,10 display:color1:trace5:data 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:TRACe<nth>:DATA? |
Return Type |
Numeric (n,n,n) |
Varies for each trace. |
|
Applicable Models: All (Read-Write) Set and return the color of data trace markers for nth trace in a window. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<nth> |
Numeric. Relative trace number in the window for which colors are set. This is not necessarily the trace number. Learn more. Choose from 1 to 8. If unspecified, <nth> is set to 1 (first trace). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:TRAC2:MARK 10,10,10 display:color1:trace5:marker 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:TRACe<nth>:MARKer? |
Return Type |
Numeric (n,n,n) |
Varies for each trace. |
|
Applicable Models: All (Read-Write) Set and return the memory trace color for nth trace in a window. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<nth> |
Numeric. Relative trace number in the window for which colors are set. This is not necessarily the trace number. Learn more. Choose from 1 to 8. If unspecified, <nth> is set to 1 (first trace). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:TRAC2:MEM 10,10,10 display:color1:trace5:memory 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:TRACe<nth>:MEMory? |
Return Type |
Numeric (n,n,n) |
Varies for each trace. |
|
Applicable Models: All (Read-Write) Set and return the color of memory trace markers for nth trace in a window. |
|
Parameters |
|
<n> |
Colors to modify. Choose from: 1 - Display colors 2 - Print colors If unspecified, <n> is set to 1 (Display colors). |
<nth> |
Numeric. Relative trace number in the window for which colors are set. This is not necessarily the trace number. Learn more. Choose from 1 to 8. If unspecified, <nth> is set to 1 (first trace). |
<num, num, num> |
Numeric. Red, Green, and Blue (RGB values) that specify a color. To find RGB values: from the Display Colors dialog, click Change Color, then Define Custom Color. |
Examples |
DISP:COL:TRAC2:MMAR 10,10,10 display:color1:trace5:mmarker 80,80,80 |
Query Syntax |
DISPlay:COLor<n>:TRACe<nth>:MMARker? |
Return Type |
Numeric (n,n,n) |
Varies for each trace. |
|