Use to change the definitions of calibration kit standards.
|
SENSe:CORRection:COLLect:CKIT: | CATalog? | CLISt | CLABel | CONNector | ADD | CATalog? | DELete | FNAMe | SNAMe | NAME | OLAB | OLISt? | ORDer | SELect | STANdard | DATA | LOAD | DELay | FMAXimum | FMINimum | LABel | LOSS | REMove | [SELect] | TYPE | TZReal | TZImag | TRLoption | LRLChar | RPLane
|
Click on a keyword to view the command details.
Blue keywords are superseded commands.
Most of these commands act on the currently selected standard from the currently selected calibration kit.
To select a Calibration kit, use SENS:CORR:COLL:CKIT:SEL.
To select a Calibration standard, use SENS:CORR:COLL:CKIT:STAN:SEL
See an example program that CREATES a New Cal Kit
See an example program that MODIFIES an Existing Cal Kit
Note: You should provide data for every definition field - for every standard in your calibration kit. If a field is not set, the default value may not be what you expect.
For more information, read Specifying Calibration Standards and Kits for Keysight Vector Network Analyzers (Application Note 1287-11)
|
Applicable Models: All (Read-only) Returns the names of the first 95 mechanical cal kits in your VNA that can be used for unguided calibrations. |
|
|
Examples |
SENS:CORR:COLL:CKIT:CAT? |
|
Return Type |
A comma-separated string |
|
Not Applicable |
|
|
Applicable Models: All (Write-Read) Assigns the calibration class for the standard |
|
|
Parameters |
|
|
<class> |
Specify the calibration classes: SA - OPEN Standards (standards in the SA class are not always Opens) SB - SHORT Standards SC - LOAD Standards THRU - Thru FWDT - Forward Trans FWDM - Forward Match REVT - Reverse Trans REVM - Reverse Match TRLT - TRL Thru TRLR - TRL Reflection TRLLm - TRL Line UTHRu - Unknown Thru ISOL - Isolation |
|
<list_stds> |
List of standard IDs (Same as SENS:CORR:COLL:CKIT:OLIS). A standard ID can be between 1 and 1000. |
|
Examples |
SENS:CORR:COLL:CKIT:CLIST SA,1,2,5 |
|
Return Type |
Numeric; returns standard number of the selected class |
|
Not Applicable |
|
Applicable Models: All (Write-Read) Defines the label for the standard classes. |
|
|
Parameters |
|
|
<class> |
Specify the calibration classes: SA - OPEN Standards (standards in the SA class are not always Opens) SB - SHORT Standards SC - LOAD Standards TRAN - Thru FWDT - Forward Trans FWDM - Forward Match REVT - Reverse Trans REVM - Reverse Match TRLT - TRL Thru TRLR - TRL Reflection TRLLm - TRL Line UTHRu - Unknown Thru ISOL - Isolation |
|
<label> |
Label of standard |
|
Examples |
SENS:CORR:COLL:CKIT:CLABEL SA,"OPEN" |
|
Return Type |
String; returns the label. |
|
Not Applicable |
|
Applicable Models: All (Write only) Creates a new connector. The connector is automatically added to the list of available connectors for the currently selected cal kit. If a connector includes both male and female connectors, each connector must be added separately. |
|
|
Parameters |
|
|
<family> |
(String) Name of connector family. Limited to 50 characters. |
|
<start> |
Start frequency |
|
<stop> |
Stop frequency |
|
<z0> |
Characteristic Impedance of the connector in ohms. |
|
<gender> |
Connector gender. Choose from: |
|
<media> |
Media of the connector. Choose from: COAX - coaxial |
|
<cutoff> |
Cutoff frequency of the connector (waveguide only). |
|
Examples |
SENS:CORR:COLL:CKIT:CONN:ADD "PSC 1.8 mm",0 HZ,999.9 GHZ,50,FEMALE,COAX,0.0 |
|
Query Syntax |
Not applicable |
|
Not Applicable |
|
|
Applicable Models: All (Read-only) Returns a comma-separated list of all connectors defined within the currently selected cal kit. The returned string includes the connector family name followed by the connector gender, if any. Kits may include a primary connector family name and additional connector family names. Connector family names are case sensitive. A connector family named "PSC 2.4" is different from a connector family named "psc 2.4". Learn more about Connector Family Name. |
|
|
Examples |
SENS:CORR:COLL:CKIT:CONN:CAT? 'Returned string "Type-N (50) male, Type-N (50) female" |
|
Not Applicable |
|
|
Applicable Models: All (Write-only) Deletes the primary connector family name from the selected kit. The VNA allows multiple connector families for each kit. If a kit includes multiple connector families, only the first listed (primary) connector family name is deleted. Once the connector family is deleted, the connector may not be assigned to any new or existing standard within the kit. The previously defined standards retain their association to the deleted connector name. To reassign standards to a new connector family name, use SENS:CORR:COLL:CKIT:CONN:SNAMe. |
|
|
Examples |
SENS:CORR:COLL:CKIT:CONN:DEL |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Replaces the primary connector family name from the selected kit with a new connector family name. The connector family name is replaced in all standards in the kit that share that name. The VNA allows multiple connector families for each kit. If a kit includes multiple connector families, only the first listed (primary) connector family name is replaced. Use the query form of this command to return the name of the primary connector family. |
|
|
Parameters |
|
|
<name> |
New connector family name. Limited to 50 characters. |
|
Examples |
SENS:CORR:COLL:CKIT:CONN:FNAM 'MYPSC35' Sense:correction:collect:ckit:connector:name 'My Type N' |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:CONNector:FNAMe? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Assigns a family name to the currently selected standard from the currently selected kit. Specify each port of a 2-port standard individually. Use the query form of this command to read the connector family name assigned to the current standard. The name is not assigned unless the connector family name is previously defined within the selected kit. |
|
|
Parameters |
|
|
<family> |
String. Connector family name. |
|
<gender> |
Connector gender. Choose from: |
|
<port> |
Number of the connector port to be assigned the connector family name. 2-port standards such as a thru line must be assigned separately. It is not relevant which connector is port 1 or port 2. 1 Specifies a 1-port standard or the first port of a 2-port standard. 2 Specifies the second port of a 2-port standard. |
|
Examples |
SENS:CORR:COLL:CKIT:CONN:SNAMe "Type-N (50)",MALE,1 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:CONNector:SNAMe? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Modifies the cal kit description field of the selected kit. This description appears in the Edit VNA Cal Kit dialog box. |
|
|
Parameters |
|
|
<string> |
Description of the cal kit. Limited to 50 characters. |
|
Examples |
SENS:CORR:COLL:CKIT:DESC "My New CalKit" |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:DESCription? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: All (Read Only) Reads characterization information from an ECal module. |
|
|
Parameters |
|
|
<module> |
Specifies which ECal module to read from. Choose from: ECAL1 .through. ECAL50 |
|
[char]
|
Optional argument. Specifies which characterization within the ECal module to read information from. If this argument is not used, the default is CHAR0. CHAR1 through CHAR5 are for user characterizations that may have been written to the module by the User Characterization feature on the VNA. Choose from: CHAR0 Factory characterization (data that was stored in the ECal module by Keysight) CHAR1 User characterization #1 CHAR2 User characterization #2 - through - CHAR12 User characterization #12 |
|
Examples |
SENS:CORR:COLL:CKIT:INF? ECAL4 |
|
|
Example return string: |
|
|
ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002 |
|
Return Type |
Character |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets a name for the selected calibration kit. |
|
|
Parameters |
|
|
<name> |
Calibration Kit name. Any string name, can include numerics, period, and spaces; any length (although the dialog box display is limited to about 30 characters). |
|
Examples |
SENS:CORR:COLL:CKIT:NAME 'MYAPC35' |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:NAME? |
|
Return Type |
String |
|
Not Applicable |
|
|
This command is replaced by SENS:COR:CKIT:CLAB. Applicable Models: All (Read-Write) Sets the label for the calibration class designated by <class>. The label is used in the prompts for connecting the calibration standards associated with that <class>. |
|
|
Parameters |
|
|
<class> |
Number of the calibration class. Choose a number between: 1 and 18. The <class> numbers are associated with the following calibration Classes: |
|
|
Class |
Description |
|
Port 1 |
|
|
|
1 |
SA |
Reflection standard |
|
2 |
SB |
Reflection standard |
|
3 |
SC |
Reflection standard |
|
4 |
FWD TRANS |
Thru/Delay standard |
|
Port 2 |
|
|
|
5 |
SA |
Reflection standard |
|
6 |
SB |
Reflection standard |
|
7 |
SC |
Reflection standard |
|
8 |
REV TRANS |
Thru/Delay standard |
|
3-port analyzers only |
||
|
Port 3 |
|
|
|
9 |
S33A |
Reflection standard |
|
10 |
S33B |
Reflection standard |
|
11 |
S33C |
Reflection standard |
|
12 |
S32T |
Thru/Delay standard |
|
13 |
S23T |
Thru/Delay standard |
|
14 |
S31T |
Thru/Delay standard |
|
15 |
S13T |
Thru/Delay standard |
|
TRL Calibrations |
||
|
16 |
TRL "T" |
Thru standard |
|
17 |
TRL "R" |
Reflect standard |
|
18 |
TRL "L" |
Line standard |
|
<name> |
Label for the calibration class. Must be enclosed in quotes. Any string between 1 and 12 characters long. Cannot begin with a numeric. |
|
Examples |
SENS:CORR:COLL:CKIT:OLAB3 'LOADS' sense:correction:collect:ckit:olabel4 'Thru' |
|
Return Type |
String |
|
Not Applicable |
|
This command is replaced by SENS:CORR:CKIT:CLIS. Applicable Models: All (Read-only) Returns seven values of standards that are assigned to the specified class. This command ALWAYS applies to the Cal Kit that is selected (using SENS:CORR:COLL:CKIT:SEL) when this ORDer command is sent. |
|
|
Parameters |
|
|
<class> |
Number of the calibration class to be queried. The <class> numbers are associated with the following calibration Classes: |
|
|
Class |
Description |
|
Port 1 |
||
|
1 |
SA |
Reflection standard |
|
2 |
SB |
Reflection standard |
|
3 |
SC |
Reflection standard |
|
4 |
FWD TRANS |
Thru/Delay standard |
|
Port 2 |
||
|
5 |
SA |
Reflection standard |
|
6 |
SB |
Reflection standard |
|
7 |
SC |
Reflection standard |
|
8 |
REV TRANS |
Thru/Delay standard |
|
3-port analyzers ONLY (N3381A/2A/3A) 4-port analyzers use S11 and S22 classes (see example program) |
||
|
Port 3 |
||
|
9 |
S33A |
Reflection standard |
|
10 |
S33B |
Reflection standard |
|
11 |
S33C |
Reflection standard |
|
12 |
S32T |
Thru/Delay standard |
|
13 |
S23T |
Thru/Delay standard |
|
14 |
S31T |
Thru/Delay standard |
|
15 |
S13T |
Thru/Delay standard |
|
TRL Calibration |
||
|
16 |
TRL "T" |
Thru standard |
|
17 |
TRL "R" |
Reflect standard |
|
18 |
TRL "L" |
Line standard |
|
Examples |
SENS:CORR:COLL:CKIT:OLIS? |
|
Return Type |
Numeric; returns the <class> number of the selected standard. |
|
Not Applicable |
|
This command is replaced by SENS:CORR:CKIT:CLIS. Applicable Models: All (Read-Write) Sets a standard number to a calibration class. This command does NOT set or dictate the order for measuring the standards. For more information, see Assigning Standards to a Calibration Class. This command ALWAYS applies to the Cal Kit that is selected (using SENS:CORR:COLL:CKIT:SEL) when this ORDer command is sent. |
|
|
Parameters |
|
|
<class> |
Number of the calibration class that is assigned to <standard>. Choose a number between: 1 and 18. The <class> numbers are associated with the following calibration Classes: |
|
|
Class |
Description |
|
|
Port 1 |
|
||
|
1 |
SA |
Reflection standard |
STAN1 |
|
2 |
SB |
Reflection standard |
STAN2 |
|
3 |
SC |
Reflection standard |
STAN3 |
|
4 |
FWD TRANS |
Thru/Delay standard |
STAN4 |
|
Port 2 |
|
|
|
|
5 |
SA |
Reflection standard |
STAN1 |
|
6 |
SB |
Reflection standard |
STAN2 |
|
7 |
SC |
Reflection standard |
STAN3 |
|
8 |
REV TRANS |
Thru/Delay standard |
STAN4 |
|
3-port analyzers ONLY (N3381A/2A/3A) 4-port analyzers use S11 and S22 classes (see example program) |
|||
|
Port 3 |
|
|
|
|
9 |
S33A |
Reflection standard |
STAN1 |
|
10 |
S33B |
Reflection standard |
STAN2 |
|
11 |
S33C |
Reflection standard |
STAN3 |
|
12 |
S32T |
Thru/Delay standard |
STAN4 |
|
13 |
S23T |
Thru/Delay standard |
STAN4 |
|
14 |
S31T |
Thru/Delay standard |
STAN4 |
|
15 |
S13T |
Thru/Delay standard |
STAN4 |
|
TRL Calibration |
|||
|
16 |
TRL "T" |
Thru standard |
STAN4 |
|
17 |
TRL "R" |
Reflect standard |
STAN1 |
|
18 |
TRL "L" |
Line standard |
STAN3 |
|
<std> |
Standard number to be assigned to the class; Choose a standard between 1 and 30. One standard is mandatory; up to six additional standards are optional. |
|
Examples |
'Assigns standard 3 to S11A class:
'Assigns standard 2 and 5 to S21T class class: |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:ORDer<class>? 'Returns only the first standard assigned to the specified class. To query the remaining standards, use SENSe:CORRection:COLLect:CKIT:OLIST[1-15]? |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: All (Read-Write) Sets and returns the name of the Cal Kit to use for Unguided cal. This command effectively does the same task as SENS:CORR:COLL:CKIT but specifies the cal kit by name. Note: During an Unguided cal, you can access ONLY mechanical cal kits #1 through #95. However, there is no limit to the number of cal kits that can be imported. |
|
|
Parameters |
|
|
<cnum> |
Currently not used. The unguided cal kit selection is for all ports on all channels. |
|
<n> |
Currently not used. The unguided cal kit selection is for all ports on all channels. |
|
<string>
|
Cal Kit name enclosed in quotes. Use SENS:CORR:COLL:CKIT:CAT? to read a list of all available Cal Kits in the VNA. |
|
Examples |
SENS:CORR:COLL:CKIT:PORT "85052B" |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:CKIT:PORT<n>:SELECT? |
|
Return Type |
String |
|
Last kit selected |
|
|
Applicable Models: All (Read-Write) Selects (makes active) a calibration kit for performing an UNGUIDED calibration or for modifying standards. All subsequent "CKIT" commands that are sent apply to this selected calibration kit. Select a calibration standard using SENS:CORR:COLL:CKIT:STAN <num>. Kits 1 to approximately kit 37 are factory installed Cal Kits. Note: During an Unguided cal, you can access ONLY mechanical cal kits #1 through #95. However, there is no limit to the number of cal kits that can be imported. This command effectively does the same task as SENS:CORR:COLL:CKIT:PORT which specifies the cal kit by name instead of this command which specifies by number. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<num> |
The number of the calibration kit. Choose from: Use SENSe:CORRection:COLLect:CKIT:RESet to restore Cal Kits to default values. |
|
|
Name |
|
1 |
Cal Kit 1 |
|
2 |
Cal Kit 2 |
|
3 |
Cal Kit 3 |
|
|
'' |
|
|
'' |
|
94 |
Cal Kit 94 |
|
95 |
Cal Kit 95 |
|
99 |
ECal module Note: Always check the list of available cal kits using SENSe:CORRection:COLLect:CKIT:CATalog? to ensure that the correct cal kit is selected. |
|
Examples |
SENS:CORR:COLL:CKIT 2 |
|
Query Syntax |
SENSe<cnum>:CORRection:COLLect:CKIT? |
|
Return Type |
Numeric |
|
Last kit selected |
|
|
Applicable Models: All (Read-Write) Sets the C0 value (the first capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for C0 in femtofarads (1E-15) |
|
Examples |
The following commands set C0=15 femtofarads: SENS:CORR:COLL:CKIT:STAN:C0 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:C0? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the C1 value (the second capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for C1. |
|
Examples |
The following two commands set C1=15: SENS:CORR:COLL:CKIT:STAN:C1 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:C1? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the C2 value (the third capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for C2. |
|
Examples |
The following two commands set C2: SENS:CORR:COLL:CKIT:STAN:C2 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:C2? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the C3 value (the fourth capacitance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for C3. |
|
Examples |
The following two commands set C3 SENS:CORR:COLL:CKIT:STAN:C3 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:C3? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the media type of the selected calibration standard. |
|
|
Parameters |
|
|
<char> |
Media type of the standard. Choose from: |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:CHAR COAX |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:CHARacter? |
|
Return Type |
Numeric |
|
Coax |
|
|
Applicable Models: All (Write-only) Loads response (and optionally accuracy) data from a file for the selected database standard. Accuracy data is loaded if the file being loaded contains accuracy data. Learn more. |
|
|
Parameters |
|
|
<string> |
Path and filename. |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:DATA:LOAD "c:\users\public\network analyzer\database_file.dat" |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the electrical delay value for the selected standard. |
|
|
Parameters |
|
|
<num> |
Electrical delay in picoseconds |
|
|
|
|
Examples |
The following two commands set delay to 50 picoseconds SENS:CORR:COLL:CKIT:STAN:DEL 50e-12 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:DELay? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the maximum frequency for the selected standard. |
|
|
Parameters |
|
|
<num> |
Maximum frequency in Hertz. |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:FMAX 9e9 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:FMAXimum? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the minimum frequency for the selected standard. |
|
|
Parameters |
|
|
<num> |
Minimum frequency in Hertz. |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:FMIN 1e3 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:FMINimum? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the characteristic impedance for the selected standard. |
|
|
Parameters |
|
|
<num> |
Impedance in Ohms |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:IMP 75 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:IMPedance? |
|
Return Type |
Numeric |
|
50 |
|
|
Applicable Models: All (Read-Write) Sets the L0 value (the first inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for L0 in femtohenries (1E-15) |
|
Examples |
The following two commands set L0=15 femtohenries: SENS:CORR:COLL:CKIT:STAN:L0 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:L0? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the L1 value (the second inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for L1. |
|
Examples |
The following two commands set L1=15: SENS:CORR:COLL:CKIT:STAN:L1 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:L1? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the L2 value (the third inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for L2. |
|
Examples |
The following two commands set L2=15: SENS:CORR:COLL:CKIT:STAN:L2 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:L2? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the L3 value (the fourth inductance value) for the selected standard. For a detailed discussion of this value, search for App Note 8510-5B at www.Keysight.com. |
|
|
Parameters |
|
|
<num> |
Value for L3. |
|
Examples |
The following two commands set L3=15: SENS:CORR:COLL:CKIT:STAN:L3 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:L3? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the label for the selected standard. The label is used to prompt the user to connect the specified standard. |
|
|
Parameters |
|
|
<name> |
Label for the standard; Must be enclosed in quotes. Any string between 1 and 12 characters long. Cannot begin with a numeric. |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:LAB 'OPEN' |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:LABel? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the insertion loss for the selected standard. |
|
|
Parameters |
|
|
<num> |
Insertion loss in Gohms / sec. (GigaOhms per second of electrical delay) |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:LOSS 3.5e9 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:LOSS? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Write only) Deletes the selected standard from the selected cal kit. |
|
|
Examples |
SENS:CORR:COLL:CKIT:STAN:REMove |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Modifies the description of the selected standard of the selected kit. This description appears in the edit kit dialog box. |
|
|
Parameters |
|
|
<string> |
Description of the standard. |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:SDES "My New Standard" |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:SDEScription? |
|
Return Type |
String |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Selects the calibration standard. All subsequent "CKIT" commands to modify a standard will apply to the selected standard. Select a calibration kit using SENS:CORR:COLL:CKIT:SEL |
|
|
Parameters |
|
|
<num> |
Number of the standard. Choose any number between: |
|
Examples |
SENS:CORR:COLL:CKIT:STAN 3 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard[:SELect]? |
|
Return Type |
Numeric |
|
1 |
|
|
Applicable Models: All (Read-Write) Sets the type for the selected standard. |
|
|
Parameters |
|
|
<char> |
Choose from: THRU (through) ARBI (arbitrary) DATabased (data-based) |
|
Examples |
SENS:CORR:COLL:CKIT:STAN:TYPE LOAD |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:TYPE? |
|
Return Type |
Character |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the TZReal component value of the Terminal Impedance for the selected standard. Note: Only applicable when the Standard Type is set to ARBI |
|
|
Parameters |
|
|
<num> |
Value for TZReal in Ohms |
|
|
|
|
Examples |
The following commands set TZReal=15 Ohms: SENS:CORR:COLL:CKIT:STAN:TZReal 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:TZReal? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the TZImag component value of the Terminal Impedance for the selected standard. Note: Only applicable when the Standard Type is set to ARBI |
|
|
Parameters |
|
|
<num> |
Value for TZImag in Ohms |
|
Examples |
The following two commands set TZImag=15 Ohms: SENS:CORR:COLL:CKIT:STAN:TZImag 15 |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:STANdard:TZImag? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All (Read-Write) Sets the reference impedance when using this TRL cal kit. Learn more. Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect. |
|
|
Parameters |
|
|
<char> |
Choose from: SYSTem - The system impedance is used as the reference impedance. During a Guided or Unguided Cal, the Z0 of the Cal standard's connector definition sets the System Z0. Make this selection when the desired test port impedance differs from the impedance of the LINE standard. Also, make this selection when skin effect impedance correction is desired for coax lines. LINE The impedance of the line standard is used as the reference impedance, or center of the Smith Chart. Any reflection from the line standard is assumed to be part of the directivity error. |
|
Examples |
SENS:CORR:COLL:CKIT:TRL:IMP SYST sense:correction:collect:ckit:trloption:impedance line |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance? |
|
Return Type |
Character |
|
LINE |
|
|
Applicable Models: All (Read-Write) This setting ONLY applies if an LRL Cal Kit is being modified AND Testport Reference Plane is set to THRU AND the TRL Thru class standard and the TRL Line/Match class standard both have the same values for Offset Z0 and Loss. Otherwise, this setting is ignored. Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect. |
|
|
Parameters |
|
|
<bool> |
Choose from: 1 or ON - Automatically correct for line loss and dispersion characteristics. 0 or OFF - Select when anomalies appear during a calibrated measurement which may indicate different loss and impedance values for the Line standards. |
|
Examples |
SENS:CORR:COLL:CKIT:TRL:LRLC 1 sense:correction:collect:ckit:trloption:lrlchar off |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar? |
|
Return Type |
Boolean |
|
OFF |
|
|
Applicable Models: All (Read-Write) Sets the reference impedance when using this cal kit. Learn more. Before sending this command, select a cal kit using SENS:CORR:COLL:CKIT:SELect. |
|
|
Parameters |
|
|
<char> |
Choose from: THRU The THRU standard definition is used to establish the measurement reference plane. Select if the THRU standard is zero-length or very short. REFLect The REFLECT standard definition is used to establish the position of the measurement reference plane. Select if the THRU standard is not appropriate AND the delay of the REFLECT standard is well defined. Also, select If a flush short is used for the REFLECT standard because a flush short provides a more accurate phase reference than a Thru standard. |
|
Examples |
SENS:CORR:COLL:CKIT:TRL:RPL THRU sense:correction:collect:ckit:trloption:rplane reflect |
|
Query Syntax |
SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane? |
|
Return Type |
Character |
|
THRU |
|