|
SENSe:SOURce | PLLBandwidth | CATalog | [:VALue] | RECeiver | CATalog | COUPling | ALL[:VALue] | [:STATe] | LIST |
|
SENSe:SOURce | RECeiver | CATalog | COUPling | ALL[:VALue] | [:STATe] | LIST |
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A (Read-Write) Lists PLL bandwidth type for SENSe<cnum>:SOURce:PLLBandwidth[:VALue]. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
Examples |
SENSe1:SOUR:PLLB:CAT? |
|
Query Syntax |
SENSe<cnum>:SOURce:PLLBandwidth:CATalog? |
|
Return Type |
<sting>, available setting list with comma separated chars |
|
Not applicable |
|
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A (Read-Write) Sets and read the settings for PLL bandwidth for RF source and LO. The source and LO settings are coupled. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<type> |
choose from:
|
|
Examples |
SENSe1:SOUR:PLLB NARR |
|
Query Syntax |
SENSe<cnum>:PLLBandwidth[:VALue]? |
|
Return Type |
Enumeration |
|
Default |
AUTO |
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A, NA520xA (Read-Write) Sets the gain settings to a specified port. Use SENS:SOUR:REC:GAIN:CAT? to return a list of available gain states for the specified port. Note: (M983xA) This command works only when the gain coupling is enabled by :SENS:SOUR:REC:GAIN:COUP:ALL. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Source port number of the VNA. If unspecified, value is set to 1 |
|
<rport> |
Receiver port number of the VNA. If unspecified, value is set to 1 |
|
<string> |
Receiver gain state. Not case sensitive. choose from:
|
|
Examples |
SENSe:SOUR1:REC2:GAIN "Low" ' Low for S21 measurement |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN[:VALue] ? |
|
Return Type |
<sting>, available setting list with comma separated chars |
|
Default |
Not |
|
Applicable Models: NA520xA (Read-Write) Sets all gains to "auto". Source/Receiver port ignored. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Ignored |
|
<rport> |
Ignored |
|
Examples |
SENSe:SOUR1:REC2:GAIN:AUT ON |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:AUT? |
|
Return Type |
Boolean (0: OFF, 1: ON) |
|
Default |
OFF |
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A, NA520xA (Read-Write) Sets the gain settings to all ports. Use SENS:SOUR:REC:GAIN:CAT? to return a list of available gain states for the VNA. Note: (M983xA) This command works only when the gain coupling is enabled by :SENS:SOUR:REC:GAIN:COUP:ALL. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Ignored |
|
<rport> |
Ignored |
|
<string> |
Receiver gain state. Not case sensitive. choose from:
|
|
Examples |
SENSe:SOUR1:REC2:GAIN:ALL "Low" ' Low for all measurements |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:ALL[:VALue] ? |
|
Return Type |
String. "MIXED" is returned when the settings are not the same. |
|
Default |
Auto |
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A, NA520xA (Read only) Reads a list of valid state for the receiver gain on the specified port. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Source port number of the VNA. If unspecified, value is set to 1 |
|
<rport> |
Receiver port number of the VNA. If unspecified, value is set to 1 |
|
Examples |
SENSe:SOUR1:REC2:GAIN:CAT? |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:CATalog? |
|
Return Type |
String (Comma-separated list of strings.) ("Auto,Low,High" is returned.) |
|
Default |
Auto |
|
Applicable Models: M983xA, NA520xA (Read-Write) Set and read the setting for receiver gain coupling for all port in the specified channel. This command does not wok for NF, NFX, SA, MOD, and MODX measurement class. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Ignored |
|
<rport> |
Ignored |
|
<Type> |
choose from:
|
|
Examples |
SENSe:SOUR1:REC:GAIN:COUP:ALL ON |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling:ALL[:VALue]? |
|
Return Type |
Enum |
|
Default |
ON |
|
Applicable Models: M983xA, NA520xA (Read only) Returns the status per port for receiver gain coupling. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Ignored |
|
<rport> |
Receiver port number of the VNA. If unspecified, value is set to 1 |
|
Examples |
SENSe:SOUR1:REC:GAIN:COUP? |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:COUPling[:STATe]? |
|
Return Type |
Boolean (0: OFF, 1: ON) |
|
Default |
ON |
|
Applicable Models: M98xxA, P50xxA/B, P93xxB, E5080B, E5081A, NA520xA (Read only) Gets the data array for actual gain setting of each measurement points. High: 1, Low: 0. The number of returned data is the same as the NOP. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<sport> |
Source port number of the VNA. If unspecified, value is set to 1 |
|
<rport> |
Receiver port number of the VNA. If unspecified, value is set to 1 |
|
Examples |
SENSe:SOUR1:REC2:GAIN:LIST? |
|
Query Syntax |
SENSe<cnum>:SOURce<sport>:RECeiver<rport>:GAIN:LIST? |
|
Return Type |
Data block |
|
Default |
Not Applicable |