Controls the Active Hot Parameters configuration.
|
SENSe:ACTive: | COMPression | BACKoff | LEVel | DELTa | X | Y | LEVel | SATuration | LEVel | DISP: | TRACe | PMAP | INPut | OUTput | SWEep: | PHASe | POINt | POWer | STARt | STEP | STOP | TYPE | TTONe: | MODE | ABSolute | RELative |
Click on a keyword to view the command details.
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the algorithm method used to compute gain compression. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<enum> |
Algorithm method. Choose from:
|
|
Examples |
SENS:ACT:COMP:ALG BACK sense:active:compression:algorithm XYcom |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:ALGorithm? |
|
Return Type |
Enumeration |
|
Default |
CFLG |
|
Applicable Models: All products with S9x111B (Read-Write) Set and read value for the BackOff compression algorithm. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Backoff value in dB. Choose a value between 1 and 99. |
|
Examples |
SENS:ACT:COMP:BACK:LEV 10 sense:active:compression:backoff:level 5 |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:BACKoff:LEVel? |
|
Return Type |
Numeric |
|
Default |
10 |
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the 'X" value in the delta X/Y compression algorithm. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
X value in dB. Choose a value from .01 to 10. |
|
Examples |
SENS:ACT:COMP:DELT:X 9 sense:active:compression:delta:X 8 |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:DELTa:X? |
|
Return Type |
Numeric |
|
Default |
10 |
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the 'Y" value in the delta X/Y compression algorithm. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Y value in dB. Choose a value from .01 to 10. |
|
Examples |
SENS:ACT:COMP:DELT:Y 9 sense:active:compression:delta:Y 8 |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:DELTa:Y? |
|
Return Type |
Numeric |
|
Default |
9 |
|
Applicable Models: All products with S9x111B (Read-Write) Sets whether or not interpolation should be performed on 2D measured compression data. Applies ONLY to 2D acquisition modes. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<bool> |
Choose from: ON or (1) Interpolate the results OFF or (0) Do NOT interpolate the results but return the value closest to compression. |
|
Examples |
SENS:ACT:COMP:INT 1 sense:active:compression:interpolate off |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:INTerpolation? |
|
Return Type |
Boolean |
|
Default |
OFF |
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the desired gain reduction (from reference gain). This value is used for Compression from Linear Gain and Compression from Maximum Gain. Use SENS:ACT:COMP:ALG CFLG to set this compression algorithm. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Compression level in dB. Choose a value between .01 and 100. |
|
Examples |
SENS:ACT:COMP:LEV 1 sense:active:compression:level 3 |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:LEVel? |
|
Return Type |
Numeric |
|
Default |
1 |
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the deviation dB from the maximum Pout. This is the point of saturation. Use SENS:ACT:COMP:ALG CFLG to set this compression algorithm. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Saturation level in dB. Choose a value between .01 and 10. |
|
Examples |
SENS:ACT:COMP:SAT:LEV 1 sense:active:compression:saturation:level 3 |
|
Query Syntax |
SENSe<ch>:ACTive:COMPression:SATuration:LEVel? |
|
Return Type |
Numeric |
|
Default |
.1 dB |
|
Applicable Models: All products with S9x111B (Read-Write) This setting is used to protect a sensitive device from too much power during the sweep retrace. Other instrument settings or channels may over-ride this setting. Learn more. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<enum> |
End Of Sweep operation. Choose from:
|
|
Examples |
SENS:ACT:EOS PSTA sense:active:eosoperation standard |
|
Query Syntax |
SENSe<ch>:ACTive:EOSoperation? |
|
Return Type |
Enumeration |
|
Default |
STANdard |
|
Applicable Models: All products with S9x111B (Read-Write) Sets whether or not interpolation is on for display. Frequency, power, and phase X axis are supported for display. Interpolation may be applied in the trace. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<bool> |
Choose from: ON or (1) Interpolate the results OFF or (0) Do NOT interpolate the results. |
|
Examples |
SENS:ACTive:DISP:INT 1 sense:active:disp:interpolation off |
|
Query Syntax |
SENSe<ch>:ACTive:DISP:INTerpolation[:STATe]? |
|
Return Type |
Boolean |
|
OFF |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read a fixed trace input power level. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<tnum> |
The number of the trace to set input power. If unspecified, the trace number is set to 1. |
|
<num> |
Input power level. The range is -10 to 0. The units are Hz, dBm, or s. |
|
Examples |
SENS:ACTive:DISPlay:TRACe1:IPWer 0 dBm sense:active:display:trace1:ipwer 0 dBm |
|
Query Syntax |
SENSe<ch>:ACTive:DISPlay:TRACe:IPWer? |
|
Return Type |
Numeric |
|
Not Applicable |
|
|
Applicable Models: All products with S9x111B (Write only) Sets the input port and output port of an Active Parameter channel. This setting is necessary only when using the limited port mapping feature. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<input> |
VNA port connected to the DUT Input. Choose from any ports with dedicated internal source. |
|
<output> |
VNA port connected to the DUT Output. Choose from any ports with dedicated internal source. |
|
Examples |
SENS:ACT:PMAP 1,3 sense2:act:pmap 1,3 |
|
Query Syntax |
Not Applicable |
|
Return Type |
Not Applicable |
|
1,3 |
|
|
Applicable Models: All products with S9x111B (Read only) Returns the VNA test port to be connected to the DUT input for an AHP channel. The SENS:ACT:PMAP sets this value. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
Examples |
SENS:ACT:PMAP:INP? |
|
Query Syntax |
SENSe:ACTive:PMAP:INPut? |
|
Return Type |
Numeric |
|
1 |
|
|
Applicable Models: All products with S9x111B (Read only) Returns the VNA test port to be connected to the DUT output for an AHP channel. The SENS:ACT:PMAP sets this value. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
Examples |
SENS:ACT:PMAP:OUT? |
|
Query Syntax |
SENSe:ACTive:PMAP:OUTPut? |
|
Return Type |
Numeric |
|
3 |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the number of phase points. For the tuning tone at the output, a phase sweep is done for each point. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Phase points. Do not exceed the max number of phase points (50). |
|
Examples |
SENS:ACTive:SWE:PHAS:POIN 201 sense:active:sweep:phase:point 101 |
|
Query Syntax |
SENSe<ch>:ACTive:SWEep:PHASe:POINt? |
|
Return Type |
Numeric |
|
8 |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the start power level for a 3D sweep. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Start power level in dBm. Choose a value from the min power to max power of the hardware. |
|
Examples |
SENS:ACTive:SWE:POW:STAR 0 sense:active:sweep:power:start 0 |
|
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STARt? |
|
Return Type |
Numeric |
|
-10 dBm |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the number of power steps for a 3D sweep. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Number of power steps. The range is 2 to 20001. |
|
Examples |
SENS:ACTive:SWE:POW:STEP 201 sense:active:sweep:power:step 201 |
|
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STEP? |
|
Return Type |
Numeric |
|
201 |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the stop power level for a 3D sweep. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Stop power level in dBm. Choose a value from min power to max power of the hardware. |
|
Examples |
SENS:ACTive:SWE:POW:STOP 0 sense:active:sweep:power:stop 0 |
|
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STOP? |
|
Return Type |
Numeric |
|
0 dBm |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the sweep type. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<char> |
Sweep type. Choose from:
|
|
Examples |
SENS:ACTive:SWE:TYPE LIN sense:active:sweep:type lin |
|
Query Syntax |
SENSe<ch>:ACTive:SWEep:TYPE? |
|
Return Type |
Character |
|
LIN |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the tuning tone mode. The tuning tone is the source at the output port to extract the X parameters. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<char> |
Tuning tone mode. Choose from:
|
|
Examples |
SENS:ACTive:TTON:MODE ABS sense:active:ttone:mode abs |
|
Query Syntax |
SENSe<ch>:ACTive:TTONe:MODE? |
|
Return Type |
Character |
|
ABSolute |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the absolute tone power level. |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Absolute tone power level. |
|
Examples |
SENS:ACTive:TTON:ABS -5 sense:active:ttone:absolute -5 |
|
Query Syntax |
SENSe<ch>:ACTive:TTONe:ABSolute? |
|
Return Type |
Numeric |
|
-5 dBm |
|
|
Applicable Models: All products with S9x111B (Read-Write) Set and read the tone power relative to the input power (dBc). |
|
|
Parameters |
|
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
|
<num> |
Relative tone power level. |
|
Examples |
SENS:ACTive:TTON:REL 10 sense:active:ttone:relative 10 |
|
Query Syntax |
SENSe<ch>:ACTive:TTONe:RELative? |
|
Return Type |
Numeric |
|
-15 dBc |
|