Sense:IF Commands


Controls the DSP filters for use with the VNA X.

SENSe:IF

| BANDwidth

| FILTer

| FILTer

| AUTO

| CMODe

| ERRors?

| STAGe

| COEFicients

| COUNt?

| FREQuency

| CATalog?

| PARameter

| TYPE

| PCATalog?

| FREQuency

| AUTO

| VALue

 

PNA-X DSP Block diagram

All of the Sense:IF commands, except the frequency commands, make settings related to the DSP section of the IF Path.

 See the entire IF Path Configuration.

  • For any of the Filter "Stage" parameters to take effect, SENS:IF:FILT:AUTO must be set to OFF (MANUAL) and mode, and SENS:IF:FILT:CMOD must be set to OFF.

  • Stage2 settings are ignored when using DSP 5 versions.

  • Programs that control these settings, or state files that are saved, will yield different results when run or recalled on VNAs with DSP 4 versions versus DSP 5 versions. Learn more about DSP versions.

  • Critical Note: These commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:Select


SENSe<cnum>:IF:BANDwidth:FILTer  <enum>

Applicable Models: N522xB and N524xB

 (Read-Write) Sets and returns the IF bandwidth filter shape. Learn more.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<enum>

(String) Filter shape. Chose from:

  • STANdard - Legacy filter. This filter has a good tradeoff between frequency selectivity and side lobes, which rise to approximately -32 dBc.

  • GAUSsian - This filter takes longer to acquire a point but has very low side lobes.

  • RECTangular - This is the fastest filter, but with high side lobes that rise to approximately -13 dBc.

Examples

SENS:IF:BAND:FILT GAUS

sense2:if:bandwidth:filter standard

Query Syntax

SENSe<cnum>:IF:BANDwidth:FILTer?

Return Type

String

Default

STANdard


SENSe<cnum>:IF:FILTer:AUTO <bool>

Applicable Models: N522xB and N524xB

(Read-Write) Sets and returns whether the VNA configures the 3-stage digital filter settings or they will be configured manually. When making manual settings, also send SENS:IF:FILT:CMOD OFF which routes the IF through the 3-stage filter.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<bool>

(Boolean)

ON (or 1) - Automatic: VNA controls digital filter settings.

OFF (or 0) - Manual: You control digital filter settings using other Sens:IF commands.

Examples

SENS:IF:FILT:AUTO 1
sense2:if:filter:auto 0

Query Syntax

SENSe<cnum>:IF:FILTer:AUTO?

Return Type

Boolean

Default

ON


SENSe:IF:FILTer:CMODe <bool>

Applicable Models: N522xB and N524xB 

(Read-Write) Sets and returns the ADC capture mode modeled as a 2-pole switch in the above diagram. The switch either bypasses or routes the IF through the 3-stage digital filter.

Critical Note

Parameters

 

<bool>

(Boolean)

ON (or 1) -  The digital filters are bypassed and the raw ADC readings are taken directly. With DSP 4 versions, a maximum of 4096 data points per sweep can be acquired.

With DSP 5 versions, the VNA maximum data points per sweep can be acquired.

Learn more about DSP Versions.

OFF (or 0) - The digital filters are used to process IF information. The filters can be configured automatically or manually using SENS:IF:FILT:AUTO.

Examples

SENS:IF:FILT:CMOD 1
sense2:if:filter:cmode 0

Query Syntax

SENSe<cnum>:IF:FILTer:CMODe?

Return Type

Boolean

Default

OFF


SENSe<cnum>:IF:FILTer:ERRors?

Applicable Models: N522xB and N524xB

(Read-only) Returns the error string associated with the digital filters. The return string has three fields separated by commas: "stage1 status, stage2 status, stage3 status"

Each of these fields can contain one or more of the following error codes:

  • NO ERROR  

  • *NUMBER-OF-COEFFICIENTS -  the number of coefficients is excessive for that filter-stage

  • *COEFFICIENT VALUE - one or more coefficients are out of range for that filter-stage

  • *SUM-OF-COEFFICIENTS - the sum of all coefficients is excessive for that filter-stage,

  • *FREQUENCY - the frequency for Stage 1 is out of range (only applies stage1 field),

  • *PARAMETER - one or more parameters are out of range (only applies to stage 3 field)

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

Examples

SENS:IF:FILT:ERR?

'example return strings"

NO ERROR, NO ERROR, NO ERROR
indicates no errors,

*SUM-OF-COEFFICIENTS, NO ERROR, NO ERROR
indicates that the sum of all filter coefficients exceed the maximum value for the Stage-1 filter,

*COEFFICIENT *SUM-OF-COEFFICIENTS, NO ERROR, *PARAMETER
indicates a problems with Stage 1 coefficients and a problem with one or more of the parameters associated with the Stage 3 filter.

Return Type

String

Default

Not Applicable


SENSe<cnum>:IF:FILTer:STAGe<n>:COEFficients <coef>

Applicable Models: N522xB, N524xB and NA520xA

(Read-Write) Sets and returns the digital filter coefficients of the specified stage.

Note: Stage2 settings are ignored when using DSP Version 5. Learn more.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<n>

Stage number. Choose 1, 2, or 3.

<coef>

Filter coefficients.

For N522xB and N524xB:

For stages 1 and 2, values can be sent as integers or in floating point format. If floating point, the values are truncated to integers. The valid range is 0 to 131071.

For stage 3: An array of floating point values. The valid range is any value within range of a floating point.

For NA520xA:

For stages 1 and 2, values can be sent as integers or in floating point format. If floating point, the values are truncated to integers. The valid range is 0 to 131071. The maximum number of coefficients is 2048. The coefficient values must be symmetrical about the center. For stage 1 the number of coefficients must be a multiple of 8. For stage 2 the number of coefficients must either be 1 or a multiple of 8.

For stage 3, values are sent in floating point format. The valid range is any value within range of a floating point. The maximum number of coefficients is 102400. The number of coefficients must be 1 or a multiple of 2.

Examples

For N522xB and N524xB:

SENS:IF:FILT:STAG2:COEF 0,0.1,0.7,0.7,0.1

sense2:if:filter:stage3:coefficients +0.0E+000,+6.4E+001,+2.56E+002

For NA520xA:

SENS:IF:FILT:STAG2:COEF 0,25960,84292,131071,131071,84292,25960,0

sens2:if:filter:stage3:coefficients +0.0E+000,+6.4E+001,+2.56E+002,+0.0E+000

Query Syntax

SENSe<cnum>:IF:FILTer:STAGe<n>:COEFficients?

Example

SENS:IF:FILT:STAG2:COEF?

Return Type

Floating point values

Default

Stage dependent


SENSe<cnum>:IF:FILTer:STAGe<n>:COUNt? [char]

Applicable Models: N522xB, N524xB and NA520xA

 (Read-only) Returns the number of taps in the digital filter of the specified stage.  The filter sample count setting is only used when SENSe:IF:FILTer:AUTO is set to False (MANUAL).

Note: Stage2 settings are ignored when using DSP Version 5. Learn more.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<n>

Stage number. Choose 1, 2, or 3

[char]

Optional parameter. Choose from:

For N522xB and N524xB:

MIN - returns the minimum number of coefficients for the specified stage. Stage1: 10, Stage2: 1, Stage3: 2

MAX - returns the maximum number of coefficients for the specified stage. Stage1 & 2: 1024, Stage3: 102400

For NA520xA:

MIN - returns the minimum number of coefficients for the specified stage. Stage1: 8, Stage2: 1, Stage3: 1

MAX - returns the maximum number of coefficients for the specified stage. Stage1 & 2: 2048, Stage3: 102400

Examples

SENS:IF:FILT:STAG2:COUN?

sense2:if:filter:stage1:count? max

Return Type

Numeric

Default

Stage dependent


SENSe<cnum>:IF:FILTer:STAGe1:FREQuency <value>

Applicable Models: N522xB and N524xB

 (Read-Write) Sets and returns the Numerically Controlled Oscillator (NCO) frequency. This command is only used when SENSe:IF:FILTer:AUTO is set to False (Manual).

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<value>

Stage 1 Frequency. Min value= 0 Hz

With DSP 4 versions, Max value= 15 MHz.

With DSP 5 versions, Max value = 38 MHz.

Or programmatically use the Max and Min queries to determine the range of settable values.

Learn more about DSP versions.

Examples

SENS:IF:FILT:STAGe1:FREQ 9e6
sense2:if:filter:stage1:frequency 9.2e6

Query Syntax

SENSe<cnum>:IF:FILTer:STAGe1:FREQuency?

'returns the current parameter value

SENSe<cnum>:IF:FILTer:STAGe1:FREQuency? Min

'returns the minimum frequency value.

SENSe<cnum>:IF:FILTer:STAGe1:FREQuency? Max

'returns the maximum frequency value.

Return Type

Numeric

Default

Nominal IF Frequency. Learn more


SENSe<cnum>:IF:FILTer:STAGe3:CATalog?

Applicable Models: N522xB and N524xB

 (Read-only) Returns a list of strings for the currently supported filter types that can be used for the stage 3 filter. This command is only used when SENSe:IF:FILTer:AUTO is set to False (Manual). See SENS:IF:FILT:STAGe3:TYPE for a list of currently supported filter types.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

Examples

SENS:IF:FILT:STAGe3:CAT?
sense2:if:filter:stage3:catalog?

Return Type

String array

Default

Not Applicable


SENSe<cnum>:IF:FILTer:STAGe3:PARameter <p>, <value>

Applicable Models: N522xB and N524xB

 (Read-Write) Sets and returns the Stage 3 filter parameters.

Must first select the filter type (SENS:IF:FILT:STAGe3:TYPE) before setting these parameters

Use SENSe:IF:FILT:STAGe3:PCAT? to return a list of the available parameters for the currently selected filter type.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<p>

(String) Filter parameter. Case Sensitive. Choose from:

"C" - Tap count (Tukey, RECT, PWIN)

"P" - Period  (PWIN ONLY)

"D" - Delay  (PWIN ONLY)

"W" - Width  (PWIN ONLY)

"R" - Ramp Count  (PWIN ONLY)

"M" - Number of times to repeat the user-supplied array for each data point (COEF ONLY)

<value>

(Numeric) Parameter Value for the specified stage 3 parameter. Use the query form to return the minimum and maximum values for the specified parameter.

Examples

SENS:IF:FILT:STAGe3:PAR "C",64

sense2:if:filter:stage3:parameter "d",0.5E-6

Query Syntax

SENSe<cnum>:IF:FILTer:STAGe3:PARameter? <p>

returns the current parameter value

SENSe<cnum>:IF:FILTer:STAGe3:PARameter? <p>,Min

returns the minimum parameter value.

SENSe<cnum>:IF:FILTer:STAGe3:PARameter? <p>,Max

returns the maximum parameter value.

Examples

SENS:IF:FILT:STAGe3:PAR? "C"

sense2:if:filter:stage3:parameter? "d",min

Return Type

Numeric

Default

RECT: C = 1

PWIN: C=1E6, P=10ms, D=50us, W=50us, R=7

TUKEY: C=1

COEF: M=1


SENSe<cnum>:IF:FILTer:STAGe3:PCATalog?

Applicable Models: N522xB and N524xB

 (Read-only) Returns a list of the available parameters for the currently selected filter type.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

Examples

SENS:IF:FILT:STAGe3:PCAT?
sense2:if:filter:stage3:pcatalog?

Return Type

String

Default

Not Applicable


SENSe<cnum>:IF:FILTer:STAGe3:TYPE <value>

Applicable Models: N522xB and N524xB

 (Read-Write) Sets and returns the Stage 3 filter type.  This command is only used when SENSe:IF:FILTer:AUTO is set to False (Manual).

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<value>

(String) Filter type. Chose from:

  • "RECT" Rectangular Window Filter

  • "TUKEY" Tukey Filter

  • "PWIN" Pulse Window Filter

  • "COEF" User-supplied array

Examples

SENS:IF:FILT:STAGe3:TYPE RECT

sense2:if:filter:stage3:type pwin

Query Syntax

SENSe<cnum>:IF:FILTer:STAGe3:TYPE?

Return Type

String

Default

"TUKEY"


SENSe<cnum>:IF:FREQuency:AUTO <bool>

Applicable Models: N522xB and N524xB

 (Read-Write) Sets and returns the method for specifying the way the IF Frequency is determined.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<bool>

(Boolean)

ON (or 1) - Automatic. VNA determines the setting for the IF frequency.  The IF frequency is based on many VNA settings, including measurement frequency. Therefore, it is NOT possible to read the IF frequency that is being used.

OFF (or 0) - Manual. Use SENS:IF:FREQ to set the frequency.

Examples

SENS:IF:FREQ:AUTO 1
sense2:if:frequency:auto 0

Query Syntax

SENSe<cnum>:IF:FREQuency:AUTO?

Return Type

Boolean

Default

ON


SENSe<cnum>:IF:FREQuency[:VALue] <value>

Applicable Models: N522xB, N524xB and NA520xA

 (Read-Write) Sets and returns the IF frequency for ALL receiver paths being used for the specified channel. To set this frequency, SENS:IF:FREQ:AUTO must be set to OFF (Manual). Also returns the maximum and minimum allowable frequency settings. Learn more.

Critical Note

Parameters

 

<cnum>

Existing channel number.  If unspecified, <cnum> is set to 1.

<value>

(Numeric) Frequency value.

For N522xB and N524xB models, the settable range is -38 MHz to +38 MHz.

For NA520xA models the settable range is -205 MHz to +205 MHz.

Note: To avoid unleveled LO errors on NA520xA models, make sure you set the IF frequency between -150 MHz and +150 MHz.

Setting a negative IF frequency: The LO frequency cannot go below 10 MHz. RF and IF frequencies determine the instrument LO frequency (LO = RF + IF). Therefore both the RF and IF frequency settings must be considered to ensure this.

Example 1: If RF is 10 MHz and LO cannot go below 10 MHz, then IF cannot go below 0 Hz (10 MHz = 10 MHz + 0 Hz).

Example 2: If RF is 100 MHz and LO cannot go below 10 MHz, then IF cannot go below -90 MHz (10 MHz = 100 MHz + -90 MHz).

For NA520xA models, once the RF frequency is greater than 215 MHz, then the IF can be set within its full range of +/-205 MHz.

For N522xB and N524xB models, once the RF frequency is greater than 48 MHz, then the IF can be set within its full range of +/-38 MHz.

Use the Max and Min Queries to determine the range of this setting. (SENS:IF:FREQ? Max)

Examples

SENS:IF:FREQ 9.1e6
sense2:if:frequency:value 8.9e6

Query Syntax

SENSe<cnum>:IF:FREQuency?

'returns the current frequency setting

SENSe<cnum>:IF:FREQuency? Max

'returns the maximum allowable frequency setting

SENSe<cnum>:IF:FREQuency? Min

'returns the minimum allowable frequency setting

Return Type

Numeric

Default

9 MHz