SENSe:ZA Commands

These commands control the compensation in the Impedance Measurement class.

SENSe:ZA

    FIXTURE

     | RESPonse:FILE

     | CKIT

          | OPEN

               | G

               | C

          | SHORt

               | R

               | L

 PORT

Click on a red keyword to view the command details.

See Also


SENSe<cnum>:ZA:FIXTure:RESPonse:FILE <FileName>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command selects the fixture (16198A-010) calibration data file (.dat) which is provided by Keysight.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<FileName>

calibration data file

Examples

SENS:ZA:FIXT:SEL "C:\Fixture_Data_xxxxxxxxx.dat"
sense:za:fixture:select "C:\Fixture_Data_xxxxxxxxx.dat"

Query Syntax

SENSe<cnum>:ZA:FIXTure:SELect?

Return Type

String

Default

Null


SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:G <value>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command sets/returns the G value of Open Standard for the fixture compensation.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

G value of Open Standard

Examples

SENS:ZA:FIXT:CKIT:OPEN:G 1e-5

sense:za:fixture:ckit:open:g 1e-5

Query Syntax

SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:G?

Return Type

Numeric

Default

0


SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:C <value>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command sets/returns the capacitance value of Open Standard for the fixture compensation.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

C value of Open Standard

Examples

SENS:ZA:FIXT:CKIT:OPEN:C 1e-5

sense:za:fixture:ckit:open:c 1e-5

Query Syntax

SENSe<cnum>:ZA:FIXTure:CKIT:OPEN:C?

Return Type

Numeric

Default

0


SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:R <value>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command sets/returns the resistance value of Short Standard for the fixture compensation.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

R value of Open Standard

Examples

SENS:ZA:FIXT:CKIT:SHOR:R 1e-5

sense:za:fixture:ckit:short:r 1e-5

Query Syntax

SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:R?

Return Type

Numeric

Default

0


SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:L <value>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command sets/returns the inductance value of Short Standard for the fixture compensation.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

L value of Open Standard

Examples

SENS:ZA:FIXT:CKIT:SHOR:L 1e-5

sense:za:fixture:ckit:short:l 1e-5

Query Syntax

SENSe<cnum>:ZA:FIXTure:CKIT:SHORt:L?

Return Type

Numeric

Default

0



SENSe<cnum>:ZA:PORT <string>

Applicable Models: All with Impedance Measurement Options (S9x041B)

(Read-Write) This command sets/returns the port for the impedance

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<string>

Port number

Examples

SENS:ZA:PORT "1"

sense:za:port "2"

Query Syntax

SENSe<cnum>:ZA:PORT?

Return Type

Numeric

Default

"1"