This program adjusts the high level amplitude response of the N5290A/91A system.
See list of supported power meters and sensors.
See VNA Accessories
|
Notes
|
Click Utility, then System, then Service, then Adjustment Routines...
At the Adjustments selection, click Receiver Characterization. The Receiver Characterization dialog is displayed as shown below.

Select the receivers to be characterized, or click Select All.
Follow the instructions displayed in the program.
The correction data is stored in the flash memory.