The Hybrid Source is a new driver selection from the External Device Configuration dialog. It combines a source with a mixer to create a high-frequency source and supports the following:
Single-Side-Band mixers
Multipliers
Note: License S94800B "Millimeter Wave Modulation" is required for any use of the Hybrid Source to output a signal with frequency greater than 90 GHz.
Note: License S94801B "Wideband Modulation" is required for the use of hybrid source to output a wideband signal that exceeds the following:
Between 4.8 GHz and 31.8 GHz, any modulation signal wider than 2.2 GHz
Between 31.8 GHz and 37 GHz, any modulation signal wider than 550 MHz
Between 37 GHz and 90 GHz, any modulation signal wider than 2.2 GHz
Once configured, an external source appears in VNA dialogs as though it were an internal source.
In this topic:
How to Configure an External Source
VNA Applications have additional methods of launching this dialog. |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
|
External Device dialog box help (Hybrid Type set to Multiplier) |
|
Hybrid TypeCurrently provides two selections: SSB Mixer (default) and Multiplier. The External Device dialog changes appearance and available settings according to the Hybrid Type you select. This section describes the External Device dialog when Multiplier is selected. Input SourceName The drop-down menu allows you to select external or internal sources. Power Limit This is the maximum power setting allowed for the Input Source, to avoid damaging the multiplier. MultiplierInput Frequency Multiplier Specify the multiplication factor here. Freq Min Minimum output frequency of the hybrid multiplier. Freq Max Maximum output frequency of the hybrid multiplier. Lock Dependent Sources (Recommended)When checked, this locks out sources that are used by this source from the GUI. By default this is checked. Note: This checkbox is already available for Hybrid SSB Mixers and now functions the same way for Hybrid Multipliers. Cal OnIf an Installation Cal has already been run, this checkbox toggles the calibration on/off. Installation CalLaunches the Hybrid Multiplier Installation Cal dialog. |
|
Hybrid Multiplier Installation Cal dialog box help (Hybrid Type set to Multiplier) |
|
This feature performs a 2D source calibration (frequency and power) on hybrid multipliers. It uses a new dynamic source calibration algorithm that determines the frequencies and powers to sample on the fly. Cal Type: Currently “Source Linearity” is the only option. Cal Using: Currently “Source PMax Table” is the only option. File: Click “…” to open a file selection dialog and select the PMax table file. The PMax table contains the saturated output powers for different frequencies. PMax file format is given below. Iteration Method: Options are "Fast," "Accurate," and "None." These determine the behavior of the dynamic source calibration algorithm.
Src Frequency Out: "Min" and "Max" give the range of frequencies over which the calibration is performed. They are not modifiable. "Nominal Step" gives the maximum measurement spacing used during calibration acquisition. If "Iteration Method" is "Fast" or "Accurate" samples may be taken with a smaller spacing. Scr Power Input: Range of input powers over which the calibration will be performed. “Nominal Step” gives the maximum measurement spacing used during calibration acquisition. If “Iteration Method” is “Fast” or “Accurate” samples may be taken with a smaller spacing. Receiver Dropdown: Select the receiver used to measure the output of the hybrid source. Cal On: If a calibration has already been run, this checkbox will toggle the calibration on/off. Last Cal: Timestamp of the most recently run calibration. Measure: Click to begin the calibration acquisition. This button is disabled until the PMax file has been loaded. PMax file format: The PMax file is a standard PRN file as exported from the PNA, but it includes one extra line at the beginning specifying the hybrid multiplier input power used to generate the table. Here is a sample: "InputPower:10dBm" |