:CALibrate:CHANnel:ENABled
Command Syntax
:CALibrate:CHANnelN:ENABled {ENABled | DISabled}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CALibrate:CHANnelN:ENABled?
Description
Enables or disables a vertical calibration for the indicated instrument's input channel.
- ENABled
-
Selects all calibrations be performed. - DISabled
-
Prevents all calibrations from being performed.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:CALibrate:CHANnel:STATus:DETails?
|
| Change in temperature | :CALibrate:CHANnel:STATus:DTEMperature?
|
| Change in Time | :CALibrate:CHANnel:STATus:TIME?
|
Query Response
{ENAB | DIS}
- ENAB
-
Indicates that all calibrations are selected. - DIS
-
Indicates that all calibrations are disabled.