:CALibrate:REMove:TCHannel
Command Syntax
:CALibrate:REMove:TCHannel CHANnel{N}
Query Syntax
:CALibrate:REMove:TCHannel?
Description
During the RemoveCable or RemoveProbe calibration wizards, this command identifies the trigger channel. You can use any analog input channel except the channel on which the cable or probe is being calibrated.