:DIFF Subsystem

The DIFF subsystem commands control differential electrical waveforms. In the :DIFF command syntax, differential waveforms are identified by the associated instrument connection number (from 1 to 8) and channel number (from 1 to 8). For example, this command sets the color of the differential waveform of an 86112A instrument installed at connections 3 and 4. Notice connection 3 channel 1 number 3_1 highlighted in red.

:DIFF3_1:COLor TCOLor8

Traditional instruments take up two connections, either connections 1 and 2 or connections 3 and 4. For these type of instruments, the differential waveform is identified using the number for the left-most occupied connection. For example, :DIFF1_1 or :DIFF3_1, respectively.

Single-connection instruments could have two channels. In this case, the differential waveform of an instrument installed at connection 4 would be identified as :DIFF4_1. Also, when Infiniium 2026 is configured with a simulated instrument, one-connection simulated instruments are available that have two channels. The following table show several examples of differential waveform identification.

Examples of Differential Waveform Numbers
Instrument Type Installed
Connections
Source Channels for
Differential Waveform
Differential Channel
Waveform Identification
Traditional Two-Connection, Dual Channel
(for example, 86112A)
1 & 2 1_1 and 2_1 :DIFF1_1
3 & 4 3_1 and 4_1 :DIFF3_1
Simulated or Future
Single-Connection, Dual Channel
1 1_1 and 1_2 :DIFF1_1
2 2_1 and 2_2 :DIFF2_1
3 3_1 and 3_2 :DIFF3_1
4 4_1 and 4_2 :DIFF4_1

Example Command Sequence

:DIFF3:DMODe ON
:CHANnel1:FILTer:BANDwidth 20E+09
:CHANnel2:FILTer:BANDwidth 20E+09
*OPC?
…
                  //  Your code to synchronize execution timing.
:DIFF3:DISPlay ON