:DISPlay:GRATicule:VDIVisions
Command Syntax
:DISPlay:GRATicule:VDIVisions <8_or_10>
<8_or_10> is an integer.
Query Syntax
:DISPlay:GRATicule:VDIVisions?
Description
This command specifies that graticules (that is, grids) have either eight or 10 major vertical divisions along the Y axis. Changing the number of vertical divisions does not affect the vertical range being displayed. Only the number of divisions used to display the vertical range is changed.
The query returns the number of vertical divisions that are currently set.
Use the :DISPlay:GRATicule:HDIVisions? command to query the number of major horizontal divisions.