:FUNCtion:PARameters:ALIGn:TIME:AUTO

Command Syntax

:FUNCtionN:PARameters:ALIGn:TIME:AUTO {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:ALIGn:TIME:AUTO?

Query Response

{1 | 0}

Description

Turns on or off automatic time-delay calculation for the Align math operator (:FUNCtion:FOPerator). To force a recalculation of the time delay, use the :FUNCtion:PARameters:ALIGn:TIME:RECalculate command. Use the :FUNCtion:FOPerator command to create an Align function.

Example Command Sequence

:FUNCtion2:FOPerator ALIGn
:FUNCtion2:PARameters:ALIGn:TIME:AUTO ON;*OPC?
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.
:FUNCtion2:PARameters:ALIGn:TIME:RECalculate

Parent Command