:FUNCtion:PARameters:BESSel:RTIMe

Command Syntax

:FUNCtionN:PARameters:BESSel:RTIMe <rise_time>

<rise_time> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:BESSel:RTIMe?

Description

For the Bessel filter operator (:FUNCtion:FOPerator), this command specifies the 10-90% rise time of the filter's step response in seconds .

This command and the :FUNCtion:PARameters:BESSel:BANDwidth command offer different ways of specifying the same filter parameter, where BW = 0.35/RT. Changing one value will set the equivalent other value.

Example Command Sequence

:FUNCtion2:FOPerator BESSel
:FUNCtion2:PARameters:BESSel:RTIMe 46.7E-12
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.