:FUNCtion:PARameters:BRICkwall:BANDwidth

Command Syntax

:FUNCtionN:PARameters:BRICkwall:BANDwidth <cutoff_frequency>

<cutoff_frequency> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:BRICkwall:BANDwidth?

Description

Specifies the cutoff frequency in Hertz of a Brickwall filter operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator BRICkwall
:FUNCtion2:PARameters:BRICkwall:BANDwidth 7.5E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.