:FUNCtion:PARameters:BUTTerworth:ORDer

Command Syntax

:FUNCtionN:PARameters:BUTTerworth:ORDer <order>

<order> is a int.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:BUTTerworth:ORDer?

Description

Specifies the order of a Butterworth filter operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator BUTTerworth
:FUNCtion2:PARameters:BUTTerworth:BANDwidth 7.5E9
:FUNCtion2:PARameters:BUTTerworth:ORDer 2
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.