:FUNCtion:PARameters:DCONvolve:FMODel

Command Syntax

:FUNCtionN:PARameters:DCONvolve:FMODel {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:DCONvolve:FMODel?

Query Response

{1 | 0}

Description

Flips the S-parameters input to an Apply S4P operator (:FUNCtion:FOPerator). If the S-parameter file's data is not defined with the ports located as shown in the top two diagrams in the following table, flip the S-parameters to ensure that the S-parameter order is properly interpreted. Use the :FUNCtion:PARameters:DEConvolve:PORDer command to ensure that the S-parameter port order is also properly interpreted.

Arguments and Dialog-Box Settings for 4-Port S-Parameters Files
Port Configuration in File Flip Model Argument
(FMODel)
4 Port Numbering Argument
(PORDer)
OFF
PORDer1324
OFF
PORDer1234
ON
PORDer1324
ON
PORDer1234

Example Command Sequence

:FUNCtion2:FOPerator DCONvolve
:FUNCtion2:PARameters:DCONvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\S-Parameter Data\DUT_4.s4p"
:FUNCtion2:PARameters:DCONvolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:PARameters:DCONvolve:PORDer PORDer1234  // Port order in file
:FUNCtion2:PARameters:DCONvolve:DRESult CMODe
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.