:FUNCtion:PARameters:DDEConvolve:CFRequency

Command Syntax

:FUNCtionN:PARameters:DDEConvolve:CFRequency <center_frequency>

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

<center_frequency> is a double.

Query Syntax

:FUNCtionN:PARameters:DDEConvolve:CFRequency?

Description

When the BANDpass filter type is selected (see :FUNCtion:PARameters:DDEConvolve:BLIMit), this command specifies the center frequency of the bandpass filter.