:FUNCtion:PARameters:GATing:REGion

Command Syntax

:FUNCtionN:PARameters:GATing:REGion {REGion{1:8}}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:GATing:REGion?

Description

Selects the region used to delimit the gating function (:FUNCtion:FOPerator). This region must be defined for the same waveform source that is the input to the function.

Example Command Sequence

:FUNCtion2:FOPerator GATing
:FUNCtion2:PARameters:GATing:REGion REGion1
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…
                  //  Your code to synchronize execution timing.