:FUNCtion:PARameters:INTerpolate:METHod

Command Syntax

:FUNCtionN:PARameters:INTerpolate:METHod {SINC | LINear}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:INTerpolate:METHod?

Description

Selects a linear or sin(x)/x interpolation for an Interpolation operator (:FUNCtion:FOPerator). The number of points in the output waveform is determined by the interpolation factor, which is set using the :FUNCtion:PARameters:INTerpolate:FACTor command.

SINC
Selects the sin(x)/x method, which is the default and is preferred when reconstructing a signal (having evenly spaced samples) that has been bandlimited. The new points are evenly spaced between the original points.
LINear
Selects the linear method.

Example Command Sequence

:FUNCtion2:FOPerator INTerpolate
:FUNCtion2:PARameters:INTerpolate:METHod SINC
:FUNCtion2:PARameters:INTerpolate:FACTor 8
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.