:FUNCtion:PARameters:SNDRatio:DISPlay
Command Syntax
:FUNCtionN:PARameters:SNDRatio:DISPlay {PAVerage | LFPResponse | SRESponse
| CPAVerage | ERRor}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtion{1:64}:PARameters:SNDRatio:DISPlay?
Description
Selects the type of waveform to display with the SNDR operator (:FUNCtion:FOPerator).
- PAVerage
- This is the source input waveform with the pattern averaging and points-per-UI linear fit math parameters applied.
- LFPResponse
- This is the (matrix) math computed linear fit pulse response p(k).
- SRESponse
- This is the step response derived from the linear fit pulse response.
- CPAVerage
- This is the Pattern Average waveform with the linear fit pulse correction applied.
- ERRor
- This is the (matrix) math computed linear fit error e(k) waveform.