:INSTrument:SIMulator:SRATe
Command Syntax
:INSTrument:SIMulator:SRATe {LOW | STANdard | HIGH}
Query Syntax
:INSTrument:SIMulator:SRATe?
Description
Selects the waveform simulation rate which affects the amount of CPU usage devoted to data simulation: LOW, STANdard, or HIGH. The default setting is STANdard. Adjusting this setting can affect the performance of Infiniium and any concurrently running applications.