:LTESt:LLINe:TEST{N}:MODE

Command Syntax

:LTESt:LLINe:TEST{1:64}:MODE {SOFailure | SOSuccess}

{1:64} identifies the specific limit line test.

Query Syntax

:LTESt:LLINe:TEST{1:64}:MODE?

Description

Specifies the event that stops data acquisition when testing limits for a limit line test are enabled. To enable testing limits, use the :LTESt:LLINe:TEST{N}:STATe command.

Command Arguments
Argument Description
SOFailure Stop data acquisition when the first failed data point occurs.
SOSuccess Stop data acquisition when the first passing data point occurs.