:MEASure:CLOCk:PPERiod:EDIRection
Command Syntax
:MEASure:CLOCk:PPERiod:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:CLOCk:PPERiod:EDIRection?
Description
For the Period - Period measurement, specifies the direction of the waveform's edges to be measured: rising or falling.
Example Command Sequence
This sequence sets up the measurement on rising edges only.
:MEASure:CLOCk:PPERiod:SOURce CHAN1_1
:MEASure:CLOCk:PPERiod:EDIRection RISing
:MEASure:CLOCk:PPERiod:NPERiods 3
// Perform measurement
:MEASure:CLOCk:PPERiod
:MEASure:CLOCk:PPERiod?