:MEASure:DATA:NOISe:MLOCation

Command Syntax

:MEASure:DATA:NOISe:MLOCation <percent>
            

<percent> is a double from 5% to 95%.

Query Syntax

:MEASure:DATA:NOISe:MLOCation?

Description

Specifies the location within the bit where the :MEASure:DATA:NOISe measurement is made. 0% is the beginning of the bit, 50% is the middle of the bit, and 100% is the end of the bit.