:MEASure:DATA:UINTerval:STATus?

Query Syntax

:MEASure:DATA:UINTerval:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the :MEASure:DATA:UINTerval measurement. Use the :MEASure:DATA:UINTerval:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:DATA:UINTerval:STATus:DETails? child query.

See Also