:MEASure:EYE:EWIDth:THReshold
Command Syntax
:MEASure:EYE:EWIDth:THReshold {AUTomatic | MTHResholds}
Query Syntax
:MEASure:EYE:EWIDth:THReshold?
Description
Selects the threshold determination method used for the :MEASure:EYE:EWIDth measurement.
-
AUTomatic— Eye Widths are measured at the widest point of the eye crossings. This measurement may be inaccurate if excessive jitter causes difficulty determining the eye crossing. -
MTHResholds— Eye Widths are measured at the measurement threshold voltage level that you specified in the Configure Measurements dialog box. This threshold may have been automatically calculated (see:MEASure:THReshold:GENeral:METHod).
Specify the threshold determination method before turning the measurement on.