:MEASure:EYE:PAM:ELEVel:LOCation?
Query Syntax
:MEASure:EYE:PAM:ELEVel:LOCation?
Description
Returns an location index of the :MEASure:EYE:PAM:ELEVel measurement for PAM or NRZ signals in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.