:MEASure:EYE:PAM:ESKew:EYE
Command Syntax
:MEASure:EYE:PAM:ESKew:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:EYE:PAM:ESKew:EYE?
Description
This command allows you to select an eye on PAM signals on which to perform the :MEASure:EYE:PAM:ESKew measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. If you experience difficulties measuring a PAM signal, confirm that the signal-type setting is set appropriately using the :CHANnel:SIGNal:TYPE command.