:MEASure:EYE:PAM:LEVel:FAVorite
Command Syntax
:MEASure:EYE:PAM:LEVel:FAVorite {ON | OFF | 1 | 0}
Query Syntax
:MEASure:EYE:PAM:LEVel:FAVorite?
Query Response
{1 | 0}
Description
Adds this measurement to, or removes it from, the Favorites category in the graphical user interface's Add Measurements dialog box.