:MEASure:EYE:PAM:LINearity:DEFinition
Command Syntax
:MEASure:EYE:PAM:LINearity:DEFinition {RLMA120 | RLMC94 | EYE}
Query Syntax
:MEASure:EYE:PAM:LINearity:DEFinition?
Query Response
{RLMA120 | RLMC94 | EYE}
Description
Selects the algorithm used to measure RML (Ratio Level Mismatch) linearity on a PAM signal. The selection arguments are:
- RLMA120
- Selects RML based upon IEEE 802.3 Annex 120D.
- RLMC94
- Selects RML based upon IEEE 802.3 Clause 94. This is the default setting.
- EYE
- Selects Eye Linearity based upon CEI.
The default value is unknown.