:MEASure:EYE:PAM:RMS:LEVel

Command Syntax

:MEASure:EYE:PAM:RMS:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}

Query Syntax

:MEASure:EYE:PAM:RMS:LEVel?

Description

Selects the eye diagram's level on which to perform the :MEASure:EYE:PAM:RMS measurement. The LEVel2 argument applies to PAM3 and PAM4 signals. The LEVel3 argument applies only to PAM4 signals. If you experience difficulties measuring a PAM signal, confirm that the signal-type setting is set appropriately using the :CHANnel:SIGNal:TYPE command.

NRZ Waveform
PAM3 Waveform
PAM4 Waveform