:MEASure:EYE:PAM:UNDershoot:STATus:REASon?

Query Syntax

:MEASure:EYE:PAM:UNDershoot:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:EYE:PAM:UNDershoot measurement. If the measurement was successful, a null string is returned. Use the :MEASure:EYE:PAM:UNDershoot:STATus? query to determine if the measurement has failed. Additional information about the failure may be available using the :MEASure:EYE:PAM:UNDershoot:STATus:DETails? query.

See Also