:MEASure:FFT:FDMagnitude:FPLevel

Command Syntax

:MEASure:FFT:FDMagnitude:FPLevel <dBm>

<dBm> is a double.

Query Syntax

:MEASure:FFT:FDMagnitude:FPLevel?

Description

Defines the threshold an FFT peak must cross to be considered a peak in the FFT Delta Magnitude measurement (:MEASure:FFT:FDMagnitude). The default Peak Level is -40 dBm.