:MEASure:FFT:FMAGnitude:FPLevel

Command Syntax

:MEASure:FFT:FMAGnitude:FPLevel <dBm>

<dBm> is a double.

Query Syntax

:MEASure:FFT:FMAGnitude:FPLevel?

Description

Defines the threshold an FFT peak must cross to be considered a peak in the FFT Magnitude measurement (:MEASure:FFT:FMAGnitude). The default Peak Level is -40 dBm.