:MEASure:HISTogram{N}:MEDian?

Query Syntax

:MEASure:HISTogram{1:4}:MEDian?

Description

Returns Median, which is the time or voltage of the point at which 50% of the histogram is to the left or right (above or below for vertical histograms) as reported on the Histograms results table.