:MEASure:HISTogram{N}:PEAK:STATus:REASon?

Query Syntax

:MEASure:HISTogram{1:4}:PEAK:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:HISTogram{N}:PEAK? measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:HISTogram{N}:PEAK:STATus:DETails? sibling query. Use the :MEASure:HISTogram{N}:PEAK:STATus? parent query to determine if the measurement has failed.

See Also