:MEASure:HISTogram{N}:PP?
Query Syntax
:MEASure:HISTogram{1:4}:PP?
Description
Returns Peak-Peak, which is the width of the histogram as reported on the Histograms results table. The width is measured as the time or voltage of the last histogram bucket with data in it minus the time or voltage of the first histogram bucket with data in it.