:MEASure:HISTogram{N}:SCALe?

Query Syntax

:MEASure:HISTogram{1:4}:SCALe?

Description

Returns the scale used to display the histogram, which is the number of hits per major graticule division. It is the Peak Hits divided by the histogram size. For vertical histograms, size is set by the :HISTogram:VSIZe command. For horizontal histograms, size is set by the :HISTogram:HSIZe command. This value is not reported on the Histograms results table.