:MEASure:HISTogram{N}:STDDev:STATus?
Query Syntax
:MEASure:HISTogram{1:4}:STDDev:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of the STDDev measurement. Use the :MEASure:HISTogram{N}:STDDev:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:HISTogram{N}:STDDev:STATus:DETails? child query.